After pressing "Configure" within the
ADC35xx GUI perform the following steps to setup HSDC pro:
- Launch HSDC Pro.
- Select the TSW1400 and click
"OK".
- Click OK for the "no firmware loaded"
prompt.
- Select “ADC3664_2W_14bit_Complex” to
load firmware, and click Yes.
- Click on the cog next to “ADC Output
Data Rate”.
- In the new dialogue box, check the
"Enable?" box.
- Under “ADC Sampling Rate”, enter
"125M".
- Under “ADC Input Frequency”, enter
"5M".
- Under "NCO", enter "4.9M".
- Under “Decimation”, enter "32".
- Click "OK".
- Select "Complex FFT".
- Press "Capture".