SBAU374A May 2021 – May 2022 DAC12DL3200
This appendix provides settings for modifying the EVM for onboard clocking mode. In this mode, no external clocks are required. The LMK04828 uses the onboard 100-MHz VCXO and the internal PLL2 to provide the required clocks along with the LMX2592.
The DAC12DL3200EVM GUI provides 12 configuration files to be used with this mode. The following list describes a few of them:
When using the "LMK_100M_LMX_6400M_Mode2_NRZ_Single_DAC.cfg" configuration file, the LMK04828 provides a 100-MHz reference clock to the LMX2592, a 50-MHz SYSREF clock to the DAC and a 400-MHz reference clock to the FPGA on the TSW14DL3200EVM.
The LMX2592 uses a 100-MHz reference clock from the LMK04828 and an internal PLL to provide the 6.4-GHz clock to the DAC. All clocks are synchronized to the 100-MHz VCXO.
To configure the DAC12DL3200EVM to use onboard clock mode, complete the following steps:
The LMK04828 routes a spare clock (DCLK10) to SMBs J26 and J28 that can be used to verify LMK operation. By default, the GUI has this clock disabled. Use the LMK04828 Clock Outputs tab to enable this clock. Set CLKout 10 and 11 DCLK Type to "LVPECL 2000 mV" and DCLK Divider to "24" to provide a 100-MHz clock to these SMBs (LMKOUTP, LMKOUTN).
The LMX2592 routes a spare clock (RFOUTB) to SMB J20 that can be used to verify LMX operation. By default, the GUI has this clock disabled. Click on the LMX2592 tab and uncheck the OUTB PD box. There is now a 6.4-GHz tone on SMB connector J20 (LMX OUT).
The LMX2582 and LMK04828 may be reconfigured to exercise more features, but this EVM is not intended to be a full evaluation platform for these devices. For a full evaluation platform, see the LMK04828EVM tool folder and LMX2592EVM tool folder.