SBAU374A May   2021  – May 2022 DAC12DL3200

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Low Latency Evaluation of Receive and Transmit
    2. 1.2 Related Documentation
      1.      Technical Reference Documents
      2.      TSW14DL3200EVM and ADC12DL3200EVM Operation
  4. 2Equipment
    1. 2.1 Evaluation Board Feature Identification Summary
    2. 2.2 Required Equipment
  5. 3Setup Procedure
    1. 3.1  Install the High Speed Data Converter (HSDC) Pro Software
    2. 3.2  Install the Configuration GUI Software
    3. 3.3  Connect the DAC12DL3200EVM and TSW14DL3200EVM
    4. 3.4  Connect the Power Supplies to the Boards (Power Off)
    5. 3.5  Connect the Signal Generators to the EVM (*RF Outputs Disabled Until Directed)
      1. 3.5.1 If External Clocking is Used (Optional)
    6. 3.6  Turn On the TSW14DL3200EVM 12-V Power and Connect to the PC
    7. 3.7  Turn On the DAC12DL3200EVM 5-V Power Supply and Connect to the PC
    8. 3.8  Turn On the Signal Generator RF Outputs
    9. 3.9  Open the DAC12DL3200EVM GUI and Program the DAC and Clocks for Single Channel, NRZ Mode 2 Operation
    10. 3.10 Open the HSDC Software and Load the FPGA Image to the TSW14DL3200EVM
    11. 3.11 DxSTRB Timing Adjustment
  6. 4Other Modes of Operation
    1. 4.1 Single-Channel RF Mode 2 (2nd Nyquist Zone)
    2. 4.2 Dual-Channel Output Mode 0
    3. 4.3 Dual Channel Mode1 Setup
    4. 4.4 Dual-Channel 2xRF Mode 0 DAC Setup
    5. 4.5 Direct Digital Synthesis Mode
  7. 5Register Log File
  8. 6Device Configuration
    1. 6.1 Tab Organization
    2. 6.2 Low-Level Control
  9.   A Troubleshooting the DAC12DL3200EVM
  10.   B DAC12DL3200EVM Onboard Clocking Configuration

Open the DAC12DL3200EVM GUI and Program the DAC and Clocks for Single Channel, NRZ Mode 2 Operation

The device configuration GUI is installed separately from the HSDC Pro installation and is a stand-alone GUI.

Figure 3-2 shows the GUI open to the LMK04828 tab. Tabs at the top of the panel organize the configuration into device and EVM features, with user-friendly controls and a low-level tab for directly configuring the registers. The EVM has three configurable devices: the DAC12DL3200, LMK04828, and LMX2592. The register map for each device is provided in the device data sheets.

Figure 3-2 illustrates the DAC12DL3200EVM GUI showing the USB status is connected to a PC.

GUID-20210330-CA0I-WC7T-FSMR-1Q86KNQT00JX-low.jpg Figure 3-2 Configuration GUI: LMK04828 Tab
  1. Open the DACDL3200EVM GUI by clicking on the DAC12DL3200 GUI icon and run as administrator.
  2. Verify the USB has connected to the board. This is indicated by a green USB Status indicator in the top right corner of the GUI. If this is not lit, click on the Reconnect? button until it does illuminate.
  3. Click on the Low Level View tab.

    Figure 3-3 illustrates loading a register configuration file to the EVM.

    GUID-20210330-CA0I-JVTT-PR7B-DHFRQTX5DMFZ-low.jpg Figure 3-3 Low Level View Tab
  4. Click on the File icon and navigate to “EXT_CLK_Mode2_NRZ_Single_DAC.cfg” and click on the OK button to load the LMK and DAC registers, see Figure 3-4.
    GUID-20210330-CA0I-PCB2-1N23-9KZCVH86LN7C-low.jpg Figure 3-4 Selecting Configuration File

This configuration file sets up the DAC to operate in a single-channel mode with the output available only on CHA. The same output is available on CHB in this mode if desired, but the configuration file has CHB powered down by default.