To set up the GUI the first time, follow these steps:
- Make sure that the previously-mentioned driver was
installed successfully to verify that everything works properly.
- Plug the connected EVM and SCB unit to the PC and go to the GUI link provided earlier.
- Click the GUI Composer application window to launch the GUI from the web browser.
- For first-time GUI Composer setup, follow the
prompts to download the TI Cloud Agent and browser extension
shown in Figure 5-5. These prompts appear after closing the README.md dialog.
- Click the
icon in the GUI Composer window to download the GUI offline (optional).