Bypass mode is the default operating mode for the
ADC32RF5x device family. When operating in this mode, the digital decimation filters
that the ADC32RF5x offers is bypassed. Additionally, the user has the option to
enable averaging of each internal pair of ADCs per individual channel. Operating in
bypass mode without averaging provides the lowest power consumption for ADC32RF5x
devices.
TSW14J58EVM
- Connect the ADC32RF5xEVM to the
TSW14J58EVM using the FMC connectors.
- Connect a 6V, 5A minimum power
supply to connector J2.
- Connect a USB 2.0 TypeA to Mini-B
cable to connector J23.
- Connect a USB 3.0 TypeA to
Micro-B cable to connector J1.
- Turn on the power supply and
toggle the power switch (SW5) to the "ON" position. The fan should start
spinning and the current draw should settle around 2.1 A.
ADC32RF5xEVM
- Connect a 12 V , 2 A minimum power supply to the connector J11.
- Connect a USB 2.0 TypeA to Mini-B
cable to connector J12.
- Connect a filtered 2.56 GHz clock
signal (+10 dBm) to input J1 (EXTCLK), then enable the signal generator
output.
- Connect a filtered 300 MHz input signal (+10 dBm) to input J3 (INA1),
then enable the signal generator output.
GUI Setup
- Open High Speed Data Converter
Pro (HSDC Pro) and select the TSW14J58. If no device is found, verify that power
is on and both USB cables are connected.
- Select the device firmware
labeled ADC32RF5x_8224_12G-16G and update the firmware by pressing
Yes on the pop-up window and waiting for the Downloading
Firmware message to finish.
- Enter 2.56 G into the ADC
Output Data Rate field. A message will appear stating "New lane rate is 12.8G
due to ADC Output Data Rate change". When this appears, press OK.
- Enter 300 M into the ADC
Input Target Frequency field and tick the checkbox "Auto Calculation of
Coherent Frequencies". You will notice that the 300M changes to 300.039
M.
- Open the ADC32RF5x GUI. Verify that the green USB Status indicator is
illuminated as shown in Figure 3-1 below. If the indicator is red (simulation mode), verify that the USB cable
is connected and that the ADC32RF5xEVM is powered on and press the Reconnect USB
button.