SBAU381A July 2021 – July 2021 TMAG5170 , TMAG5170 , TMAG5170-Q1 , TMAG5170-Q1 , TMAG5173-Q1 , TMAG5173-Q1 , TMAG5273 , TMAG5273
Item |
Description |
Quantity |
---|---|---|
Clip On Base |
Base.STL |
1 |
Orbital Arm |
Arm.STL |
1 |
Orbital Slider |
Slider.STL |
1 |
1/4" dia. x 3/16" thick Cylindrical magnet |
NdFeB (N52): available at K&J Magnetics |
1 |
1" 4-40 Hex Socket screw |
Nylon screw: available at McMaster Carr |
1 |
4-40 Hex Nut |
Nylon Hex Nut: available at McMaster Carr |
2 |
4-40 Stand off: 1/4" |
Nylon Hex Standoff: available at McMaster Carr |
1 |
8333-20G |
Super Glue |
0.02 oz |
4-40 Stand off: 1/16" |
Nylon Hex Standoff: available at McMaster Carr |
1 (optional) |
1/4" 4-40 screw |
Nylon screw: available at McMaster Carr |
1 (optional) |
Step 1- Print the Orbital Slider (Slider.STL)
This is the printable slider for the orbital attachment. Notice the indented seat for the set screw nut and for an optional slider clamp screw.
Step 2 - Glue in the 4-40 Hex nut in the center set screw opening
Glue the Hex nut in the center opening shown below. Additionally, glue in the 1/16" 4-40 standoff in the off center clamp screw indentation if desired.
Step 3 - Print the Orbital Arm (Arm.STL)
This is the central fixture of the assembly. It will clip into the attachment base and serves as a guide for the slider assembly already printed.
Step 4 - Guide the Orbital Slider onto the Orbital Arm
Figure 2-5 shows how the slider can easily slide onto the top of the arm.
Step 5 - Insert the set screw
Insert the set screw from the inside of the Orbital Arm. This will serve as both a handle and a control for the range of the magnet.
Figure 2-7 shows the how the set screw should appear at full extension.
Step 6 - Glue the magnet, remaining hex nut, and 1/4" standoff to set screw
With these items attached, the set screw will no longer be removable from the assembly and the slider will be permanently connected. With the magnet centered on the screw head, the pole of the magnet will be continuously directed towards the sensor location. If desired, it is possible to attach any reasonably sized magnet here, but take care to ensure a pole is directed towards the device. The magnet may be oriented with either pole facing the sensor, but it is necessary to be consistent when correlating position to the observed field.
Step 7 - Print the Clip on Base (Base.STL)
This printable piece will serve to connect the attachment to the EVM. The sensor platform will slide through the opening and then may clip onto the circular guides on the base.
Step 8 - Connect the Base to the Orbital Arm
This connection will complete the assembly of the attachment and allow the sensor to move at a fixed radius.