To set up the GUI the first time,
follow the below instructions:
- Make sure that the above
mentioned driver was installed successfully to ensure that everything works
properly and that the GUI can update the EVM firmware, if necessary.
- With the EVM/TI-SCB Controller
unit plugged to the PC, go to the GUI link provided above.
- To launch the GUI from the web
browser, click the GUI Composer application to open the GUI
Composer window (see Figure 4-4).
- For first-time GUI
Composer setup, follow the prompts to download the TI Cloud
Agent and browser extension shown in Figure 4-5.
These prompts will appear after you close the README.md dialog.
- Optionally, the GUI can be
downloaded for offline use by clicking the
icon in
the GUI Composer window shown in Figure 4-4.