SBAU400 November 2023 TMAG5253
This EVM allows the user to evaluate the TMAG5253. The EVM includes a trigger attachment that controls the perceived brightness of an onboard RGB LED according to the analog output of the TMAG5253. The EVM is intended to provide basic functional evaluation of the devices. The layout is not intended to be a model for the target circuit, nor is it laid out for electromagnetic compatibility (EMC) testing.