SBAU407 april 2023 ADS8354
Figure 3-3 shows the signal path for the analog inputs applied to the ADS8354EVM. Separate THS4561 amplifiers are used with a gain of 1 V/V configuration to drive the individual analog inputs (AINP and AINM) of each ADC. The OPA320 amplifier circuits help drive the common-mode voltage (VOCM) of the THS4561 amplifiers. An RC filter, with values of Rfilt = 13 Ω, differential Cfilt = 820 pF, and common-mode Cfilt = 10 pF, was selected to achieve a SINAD greater than 88 dB and a THD less than –97 dB for a 2-kHz sine-wave input at full throughput of the ADS8354 of 700 kSPS.
As shown in Figure 2-2, the ADS8354EVM offers two options to provide the output common-mode voltage (VOCM) of the THS4561 amplifiers. By default, JP7 and JP8 are left open and JP5 and JP6 are installed. This configuration selects the ADS8354 internal reference voltage (REFIO_A and REFIO_B) and divides the output by 2 to use REFIO_y / 2 as VOCM (y = A or B), which is required for the default input range of ±VREF. When using the 2xVREF input range, uninstall the jumpers on JP5 and JP6 such that VOCM = REFIO_y.
Alternatively, the REF6025 (U1) can be used in place of the REFIO_A, REFIO_B voltage to serve as the ADC reference and to set the VOCM voltage. Disable the internal reference voltage on the ADS8354 by setting the REF_SEL bit in the CFG register to 0b (external reference) and install jumpers on JP7 and JP8.