SBAU408 august   2023 ADS7953

 

  1.   1
  2.   ADS7953EVM-PDK Evaluation Module
  3.   Trademarks
  4. 1Overview
    1. 1.1 ADS7953EVM-PDK Features
    2. 1.2 ADS7953EVM Features
  5. 2Analog Interface
    1. 2.1 Connectors for Analog Inputs
    2. 2.2 ADC Input Signal Driver
      1. 2.2.1 Input Signal Path
  6. 3Digital Interfaces
    1. 3.1 SPI for the ADC Digital I/O
  7. 4Power Supplies
    1. 4.1 ADC Voltage Reference Configuration
  8. 5ADS7953EVM-PDK Initial Setup
    1. 5.1 Default Jumper Settings
    2. 5.2 EVM Graphical User Interface Software Installation
  9. 6ADS7953EVM-PDK Operation
    1. 6.1 EVM GUI Global Settings for ADC Control
    2. 6.2 Time Domain Display Tool
    3. 6.3 Spectral Analysis Tool
    4. 6.4 Histogram Analysis Tool
    5. 6.5 Device Configuration
    6. 6.6 Alarm Configuration
  10. 7Schematic, Bill of Materials, and Printed-Circuit Board Layout
    1. 7.1 Schematic
    2. 7.2 Bill of Materials
    3. 7.3 PCB Layout

Alarm Configuration

The Alarm Configuration page (Figure 6-7) sets the alarm thresholds of the ADS7953 ADC. The device has an alarm feature that allows GPIO0 to be configured as either a high or low or just as a low alarm threshold and GPIO1 to be configured as a low alarm threshold. These GPIO configurations can be set by going to the Device Configuration page and using the drop-down menu to select the appropriate function for the two GPIOs. In the GUI, these thresholds are set using a 12-bit hexadecimal value and are available on all 16 channels. If a threshold is crossed, the bell under GPIO0 or GPIO1 illuminates depending on which threshold is crossed and the configuration of the two GPIOs. To program the values, enter the appropriate threshold value and click on the Program Alarm Registers button. Only channels 0 to 7 are displayed by default. To set the thresholds for the other eight channels, click the CH8-CH15 button next to Select Page at the bottom right corner of the window.

GUID-20221007-SS0I-ZKNQ-FMRV-RPVMB7MQT0XT-low.svgFigure 6-7 Alarm Configuration Page