The following instructions are a step-by-step guide for connecting the device to a computer and evaluating the performance of the device.
- Connect the device EVM to the PHI board.
- Use the provided USB cable to connect the PHI to the computer.
- LED D5 on the PHI lights up, indicating that the PHI is powered up.
- LEDs D1 and D2 on the PHI start flashing, indicating that the PHI is booted up and communicating with the PC.
- Launch the device EVM GUI software from the installed path, as Figure 6-1 shows, or by using the desktop shortcut created during installation.