SBAU408 august 2023 ADS7953
Figure 2-1 shows the signal path for the analog inputs applied to the ADS7953EVM. A separate OPA192 amplifier is used in a unity-gain buffer configuration to drive the individual analog input of channel 15 (CH15). An additional OPA192 is connected from the internal multiplexer output (MXO) to the ADC input (AINP). Onboard provisioning enables both OPA192 amplifiers to be bypassed with configurable jumper options listed in Table 5-1. An RC filter with values of 33 Ω and 270 pF was selected to achieve a optimal performance at full throughput (1 MSPS) of the ADS7953.