The following instructions are a step-by-step guide to connecting the ADS131B26Q1EVM-PDK to the computer and evaluating the performance of the ADS131B26-Q1:
- Review the default jumper settings in Section 5.1 and GUI software installation in Section 5.2.
- Connect the ADS131B26Q1EVM-PDK to the PHI controller. Install the two screws as indicated in Figure 1-1.
- Connect the PHI controller to your PC using the
provided USB micro cable. Three LEDs illuminate on the PHI controller to
indicate connectivity to the PC.
- LED D5 lights up solid, indicating that the PHI is
powered up.
- LEDs D1 and D2 start blinking at different rates to
indicate that the PHI is booted up and communicating with the PC. Figure 1-1
shows the resulting LED indicators.
- Launch the ADS131B26Q1EVM-PDK GUI software and power is supplied to the EVM.
The default installation path is C:\Program Files (x86)\Texas
Instruments\ADS131B26-Q1 EVM.
- When the GUI finishes loading and is connected to the EVM hardware, the
screen appears as illustrated in Figure 6-1. The GUI consists of multiple Pages, which
include:
- Register Map Config
- Time Domain Display
- Spectral Analysis
- Histogram Analysis
- Channel
Configurations
- Sequencer
Configurations
Below the Pages section are the basic SPI op-code commands, the
Data Capture Configuration controls, and the current Clocks and
Data Rate information. Section 6.1 details the EVM GUI pages and data capture controls.