SBAU422 November 2023 TMCS1126
The following are instructions to set up and use the TMCS1126xEVM. Figure 2-1 shows an example of a simple, low-side setup on the A1 (25 mV/A) sensitivity variant. This device has isolation, and external supplies are distinguished by high voltage (HV) for load and low voltage (LV) for DUT supply. The HV supply can be isolated and at a different potential than the LV supply.
When measuring current, first make sure that equipment (wires, connectors, etc.) can support the amperage and power dissipation. Secondly, make sure that current flowing through the inputs of the device is kept within the safe operating area limits of the device found in the TMCS1126 data sheet. Failure to do so can result in damage to the EVM, or personal injury.
Do not touch the HV terminals
Hot surface. Contact can cause burns. Do not touch!