SBAU432 December   2023 AFE7728D , AFE7768D , AFE7769D

 

  1.   Abstract
  2.   2
  3.   Trademarks
  4. 1Introduction
  5. 2Basic EVM Test Procedures
    1. 2.1 Safety
    2. 2.2 Quality
    3. 2.3 Apparel
    4. 2.4 Hardware and Software Requirements
      1. 2.4.1 Test Equipment Required
      2. 2.4.2 Software Required
  6. 3AFE7769DEVM Setup
    1. 3.1 AFE7769D Hardware Changes
    2. 3.2 AFE7769D Connections
    3. 3.3 AFE7769D Software Setup
    4. 3.4 AFE7769D Programming Method 1: Automated
    5. 3.5 AFE7769D Programming Method 2: Using GUI Mode

AFE7769D Programming Method 2: Using GUI Mode

  1. Open the AFE77xxD GUI version 0.4. Make sure it looks like Figure 3-8, then click Continue. The “Couldn’t Detect FPGA Reset FTDI. Please reset FPGA manually.” message is expected and can be ignored.
    GUID-20230731-SS0I-CT7F-FKPG-90JJT85GN6QQ-low.png Figure 3-8 Launching AFE77xxD Latte Software
  2. Wait until the GUI loads. It will look like Figure 9. Click on “AFE77xxD-Device” tab under the tree view on the left for the main parameters screen.
    GUID-20230731-SS0I-XB3V-PLKG-JRDLWBC5VD9J-low.png Figure 3-9 ReadMe AFE77xxD Latte Software
  3. Click on “Browse” under “Load System Parameters” and select the “AFE77xxD_Picocom_pc802_K1L.xlsx” config file under “\Documents\Texas Instruments\AFE77xxDLatte\lib\configs”. After selecting the file, click “LOAD”, and the screen should look like Figure 3-10. You should also see a message saying that the configuration was loaded in the log window.
    GUID-20230731-SS0I-F6P9-MM6L-VTBRKBCTTMDX-low.png Figure 3-10 Main Window: GUI Mode
  4. Set the LMK parameters on the bottom left corner like Figure 3-11.
    GUID-20230731-SS0I-XQCL-DVQK-9WKGJCHF41JC-low.png Figure 3-11 Setting LMK Parameters
  5. After that, under “Hardware Connection”, click the refresh GUI button and you will see a message on the log window saying “Refreshed GUI”. Then click on “Device Bringup” this will start the bring up for the device. For proper navigation, see Figure 3-12.
    GUID-20230731-SS0I-6JDC-MP9B-PBQSHS8HRTGS-low.png Figure 3-12 Device Bringup
  6. After the device bringup is done, you will see some errors on the log window (shown in Figure 3-13). Two of these errors should be “FPGA Reset device not found” and the rest should be under the “Device DAC JESD-RX 0 Link Status” line. These errors are expected since the JESD link is not up.
    GUID-20230731-SS0I-CF4S-BM9G-7RF8GCNQWSKV-low.png Figure 3-13 Latte Log Qindow Post-Bringup
  7. At the top, click on Latte Mode and navigate to Script Mode as shown in Figure 3-14.
    GUID-20230731-SS0I-VFLN-NKDW-N1NR0Z9SLPT7-low.png Figure 3-14 Switching to Script Mode
  8. Open the PC802_LMKDIV.py script on the tree view on the left, as shown in Figure 3-15.
    GUID-20230731-SS0I-R5VP-G7VL-NBZMRMRX0PLP-low.png Figure 3-15 PC802 LMK Script
  9. Run the script by pressing F5 or by clicking Run > Buffer. You should see an output in the log window like Figure 3-16, signaling the script was run with no errors. After running this script, the LMK_LOCKED LED (D11) turns on if the 122.88 MHz reference from the PC802 is connected.
    GUID-20230731-SS0I-JKLH-FPR3-GX4GRMVPRDHG-low.png Figure 3-16 Running the LMK Script
  10. Click on Latte Mode and navigate to GUI Mode as shown in Figure 3-17.
    GUID-20230731-SS0I-KXH4-858F-4D6RRZ5PXCLV-low.png Figure 3-17 Switching to GUI Mode
  11. Click on “TX-Test” under the tree view, as shown in Figure 3-18.
    GUID-20230731-SS0I-HXLJ-QHBN-SSTPTB70PBM0-low.png Figure 3-18 Switching to TX-Test Tab in Latte
  12. Enable the TDD for the TX channels by setting them to green like in Figure 3-19. Then, click “Set TX TDD”, and a message should appear on the log window that says “TDD set”.
    GUID-20230731-SS0I-RF4W-F4S9-8QZFJQXQ534L-low.png Figure 3-19 Enabling TDD Mode
  13. Proceed to set up the PC802 by following the PC802 EVB RFIC Demonstration User Guide (Version 3) (where is this doc located or what is the lit number?) from section 2.2. Once you get to section 2.2.5, after you enter the “start” command on the test mode tool to start sending data, type the “AFE.adcDacSync(1)” command in the Command line in the AFE77xxD GUI. You should now be able to see a report in the log window that the JESD link is up with no errors like in Figure 3-20. Data will be going out of the AFE TX channel.
    GUID-20230731-SS0I-NST2-98Z7-W38CPHL6MS9S-low.png Figure 3-20 JESD Link Bringup