Connect the EVM as shown in Figure 5-1 after installing the software:
- Physically connect P2 of the PHI to J5 of the ADS1278 EVM.
- Install the screws to provide a robust connection. Connect the USB on the PHI to the computer.
- LED D5 on the PHI lights up, indicating that the PHI is powered up.
- LEDs D1 and D2 on the PHI start blinking to indicate that the PHI is booted up and communicating with the PC.
- Power the ADS1278 EVM through the J10 terminal with 6V.
- Start the software GUI. Notice that the LEDs on the PHI blink slowly when the FPGA firmware is loaded on the PHI. Loading takes a few seconds.
- Connect the signal generator. The input range is
0V to 5V. A common input is a 4.9VPP signal with a 2.5V offset. This
signal is adjusted just below the full-scale range to avoid clipping.