- Connect the ADC3910D125EVM to the TSW1418EVM
through the FMC connector.
- Connect the FTDI board to the ADC3910D125EVM onto
J2 of the ADC3910D125EVM.
- Install the JTAG dongle provided with the
TSW1418EVM onto J3 of the TSW1418EVM.
- Make sure J13 on TSW1418EVM is between pin two
and three.
- Connect a +12V power supply to the barrel
connector (power supply cable included with EVM) of the ADC3910D125EVM.
- Connect a mini USB cable from the PC to the FTDI
board installed on the ADC3910D125EVM.
- Connect a mini USB cable from the PC to J2 on the
TSW1418EVM.
- Connect a micro USB cable from the PC to the JTAG
dongle (on the TSW1418EVM) that was installed in step three.
- Connect a bandpass filtered clock signal source
to J7 labeled CLK of the ADC3910D125EVM.
- Connect a bandpass filtered analog input source
to J8 and/or J10 of the ADC3910D125EVM labeled INAp and INBp, respectively.
If all the steps above were followed correctly,
then the final setup looks like the following: