The following instructions are a step-by-step guide for connecting the ADS8681WEVM-PDK to the computer and evaluating the performance of the ADS8681W:
- Connect the ADS8681WEVM to the PHI. Install the two screws as indicated in Figure 4-1.
- Use the provided USB cable to connect the PHI to the computer
- LED D5 on the PHI lights up indicating that the PHI has powered up
- LEDs D1 and D2 on the PHI start blinking, indicating the PHI is booted up and communicating with the EVM
- Launch the ADS8681EVM GUI software from the Start Menu of computer, Desktop Shortcut, or Installation folder (Figure 4-2).