SBAU480 November 2024
The following are instructions to set up and use the INA75xEVM. Figure 3-1 shows an example of a simple, high-side setup . The high voltage source for load is noted as VCM. The low voltage DUT supply is noted as VS. The shorting jumpers A, B and C are installed such that VREF equals to GND and the DUT gain is 80mV/A.
When measuring current, first make sure that equipment (wires, connectors, and so forth) can support the amperage and power dissipation. Secondly, make sure that current flowing through the inputs of the device is kept within the safe operating area limits of the device found in the device data sheet. Failure to do so can result in damage to the EVM, or personal injury.
Do not touch the high voltage VCMterminals.
Hot surface. Contact can cause burns. Do not touch.