SBOA444 November 2020 TMCS1100
Each of the ADS131M08 converters is differential and requires that the input voltages at its pins does not exceed ±1.2 V (assuming an internal PGA gain setting of 1 is used). To meet this input voltage specification, a voltage and current sensor circuit is needed to translate the Mains voltage and outlet current into a voltage that can be sensed by the ADS131M08. This subsection describes the analog front end used for voltage and current channels.