SBOA444 November   2020 TMCS1100

 

  1.   Trademarks
  2. 1Introduction
  3. 2Implementation Block Diagram
  4. 3Hardware Implemenation
    1. 3.1 Analog Inputs
      1. 3.1.1 Voltage Measurement Analog Front End
      2. 3.1.2 Current Measurement Analog Front End
    2. 3.2 MSP432 LaunchPad Connections
    3. 3.3 PCB Layout Recommendations
  5. 4How to Implement Software for Metrology Testing
    1. 4.1 Setup
      1. 4.1.1 Clock
      2. 4.1.2 UART Setup for GUI Communication
      3. 4.1.3 Real-Time Clock (RTC)
      4. 4.1.4 Direct Memory Access (DMA)
      5. 4.1.5 ADC Setup
    2. 4.2 Foreground Process
      1. 4.2.1 Formulas
        1. 4.2.1.1 Standard Metrology Parameters
        2. 4.2.1.2 Power Quality Formulas
    3. 4.3 Background Process
      1. 4.3.1 per_sample_dsp( )
        1. 4.3.1.1 Voltage and Current ADC Samples
        2. 4.3.1.2 Pure Waveform Samples
        3. 4.3.1.3 Frequency Measurement and Cycle Tracking
      2. 4.3.2 LED Pulse Generation
      3. 4.3.3 Phase Compensation
  6. 5Metrology Accuracy Testing
    1. 5.1 Test Setup
    2. 5.2 Results
  7. 6Schematics
  8. 7References

Direct Memory Access (DMA)

The direct memory access (DMA) module transfers packets between the MSP432 and ADS131M08 device with minimal bandwidth requirements from the MSP432 CPU. Two DMA channels are used for communicating to the ADS131M08. One channel (channel 0) is used to send data to the ADS131M08 and the other channel (channel 1) is used to receive data from the ADS131M08. Once a complete packet has been received from the ADS131M08, an interrupt is generated to complete any necessary post-transfer processing, such as CRC verification and packet assembly. The ADS131M08 ADC Sample Request Packet figure shows the packets that are sent and received using the DMA of the MSP432.