The effect of heavy-ion irradiation on the single-event effects performance of the TRF0206-SP high-performance, differential amplifier is summarized in this report. Heavy-ions with an LETEFF up to 82.1 MeV-cm2/mg were used to irradiate two production devices in multiple runs. Flux up to 105 ions/cm2-s and fluences up to 107 ions/cm2 at temperatures of 25°C (SET) and 125°C (SEL), were used for the characterization. Results demonstrate that the TRF0206-SP is SEL-free up to LETEFF = 82.1 MeV-cm2/mg and 125°C, and the cross section for the SET is discussed.
LabView™ is a trademark of National Instruments Corporation.
DuPont® and Kevlar® are registered trademarks of E.I. du Pont de Nemours and Company.
All trademarks are the property of their respective owners.