SBOA564A December   2022  – August 2024 TRF0206-SP

 

  1.   1
  2.   Single-Event Effects Test Report of the TRF0206-SP 6.5-GHz Differential Amplifier
  3.   Trademarks
  4. Overview
  5. Single-Event Effects
  6. Test Device and Evaluation Board Information
  7. Irradiation Facility and Setup
  8. Depth, Range, and LETEFF Calculation
  9. Test Set-Up and Procedures
  10. Single-Event Latch-up (SEL) Results
  11. Single-Event Transients (SET) Results
  12. Event Rate Calculations
  13. 10Summary
  14.   A Total Ionizing Dose from SEE Experiments
  15.   B Confidence Interval Calculations
  16.   C Orbital Environment Estimations
  17.   D References
  18.   E Revision History

Total Ionizing Dose from SEE Experiments

The production TRF0206-SP POL is rated to a total ionizing dose (TID) of 100 krad(Si). In the course of the SEE testing, the heavy-ion exposures delivered ≅ 1 krad(Si) per 106 ions/cm2 run. The cumulative TID exposure for each device respectively, over all runs they each underwent, was determined to be greater than 100 krad(Si). The two production TRF0206-SP devices used in the studies described in this report stayed within specification and were fully-functional after the heavy-ion SEE testing was completed.