SBOA570 may 2023 LMC6061 , LMC6081 , OPA192 , OPA2277 , OPA2350 , OPA277 , OPA320 , OPA328 , OPA350 , OPA391 , OPA392 , OPA4277 , OPA4350
Very low current noises do not impact overall noise performance unless the source impedance is very large. In the case of a 1fA/√Hz current noise, the source resistance needs to be greater than 16.5 GΩ for current noise to make a significant contribution to overall noise. For CMOS and JFET devices, it is common for current noise to increase at higher frequencies. This increase in current noise is called f-squared noise. Circuits where the source impedance is high limit, the bandwidth below the frequency where current noise begins to increase. This bandwidth limitation tends to counterbalance the impact of the f-squared noise so that the total RMS noise is not impacted significantly by the f-squared noise.