SBOA580 November 2023 INA1620 , OPA1602 , OPA1604 , OPA1611 , OPA1612 , OPA1612-Q1 , OPA1622 , OPA1632 , OPA1655 , OPA1656 , OPA209 , OPA210 , OPA211 , OPA211-EP , OPA2209 , OPA2210 , OPA2211-EP , OPA2211-HT , OPA2211A
Figure 3-7 shows a test circuit used to measure THD + N of the inverting amplifier configuration. The input signal Vin to the amplifier is provided by the generator output. The input offset voltage Vos and the input voltage noise Vn are series error sources internal to the op-amp. Vos and Vn are always referred to the non-inverting terminal and both are amplified by the noise gain of the amplifier configuration.
Superposition is used to derive separate equations for the signal gain and the distortion gain of the inverting distortion test circuit shown in Figure 3-7. Assuming the input offset voltage Vos = 0 V, the noise voltage Vn = 0 V, and the current iRA = 0 A the amplifier configuration shown in Figure 3-7 can be viewed as the standard inverting amplifier configuration as shown in Figure 3-8. The signal gain magnitude is determined by the ratio of resistor RF to resistor RB. Equation 8 represents the signal gain of the inverting distortion test circuit. The concept of a virtual short is assumed when removing resistor RA. The voltage potential across resistor RA on the inverting and non-inverting terminals are equal when applying the concept of a virtual short and therefore iRA = 0 A and RA is viewed as an open.
Figure 3-9 represents the THD + N gain circuit. Assuming Vin = 0 V, resistors RA and RB are in parallel. The amplifier can be observed as a standard non-inverting amplifier with the addition of resistor RA. The voltages Vos + Vn are applied at the non-inverting terminal. Vos + Vn appear at the output gained up by the familiar non-inverting gain equation of one plus the ratio of resistor RF to RA|| RB. Equation 9 represents the THD + N gain of the inverting distortion test circuit.
Equation 10 is found by expanding Equation 9.
The signal observed on the output of the test circuit shown in Figure 3-7 is the amplified combination of Vin, Vn and Vos and is represented by Equation 11. Equation 11 represents the final gain equation of the inverting distortion test circuit shown in Figure 3-7.
The typical inverting circuit does not
include the additional resistor RA. Resistor RA was added to
the test circuit to provide additional gain for the purpose of overcoming the signal
analyzer measurement limitation. Table 3-2 assigns values to resistors RF, RA and RB and
the associated gain values for both the test circuit and application circuit are
calculated. With the assigned resistor values in Table 3-2 the THD + N gain is
with the addition of resistor RA. In the common inverting
application circuit RA =
, or in other words doesn't exist and the
THD
+ N gain is
. Therefore RA added an additional
or approximately 34 dB of distortion gain.
Condition | Signal Gain | THD + N Gain | RF | RA | RB |
---|---|---|---|---|---|
Signal & THD + N Gain with RA | 10 kΩ | 100 Ω | 10 kΩ | ||
Signal & THD + N Gain without RA | 10 kΩ | 10 kΩ |
Figure 3-10 shows the measured THD + N ratio of the OPA1656 in units of decibels. 34 dB is subtracted from the test circuit measurement and represents the actual op amp THD + N that is seen in the typical inverting circuit. The measurement bandwidth of the distortion analyzer is 80 kHz.
Figure 3-11 shows the THD + N (%) ratio vs Output Amplitude (VRMS) for the common inverting application circuit. Two independent measurements were made for 1 kHz and 20 kHz frequencies as the output amplitude was swept from 0.1 VRMS to 10 VRMS.