SBOA580 November 2023 INA1620 , OPA1602 , OPA1604 , OPA1611 , OPA1612 , OPA1612-Q1 , OPA1622 , OPA1632 , OPA1655 , OPA1656 , OPA209 , OPA210 , OPA211 , OPA211-EP , OPA2209 , OPA2210 , OPA2211-EP , OPA2211-HT , OPA2211A
Op amp distortion can be considered an internal error source that can be measured by observing changes of the input offset voltage Vos and how these changes in Vos alter the signal of interest Vin. The Vos of an amplifier is the difference between the inverting and non-inverting inputs. Fluctuations in Vos are small when operating within the linear region of the amplifier. Examples that can directly or indirectly cause a change between the op amp inputs or Vos are but not limited to temperature drift, common mode and power supply voltage fluctuations, slew rate, and reduction in open loop gain or Aol. Aol is dependent on frequency. Ignoring the Aol frequency dependency, Equation 2 shows the relationship between Vos, Vout and Aol.
Equation 3 is found by rearranging Equation 2. Two observations are made from Equation 3, and . These observations show that Aol is responsible for correcting amplifier errors. Parts with high open loop gain create less Vos errors. In theory a virtual short of an op amp is when the inverting and non-inverting terminals have equal voltage potentials even though there is no connection between them. The assumption is used in the following sections when applying the principles of superposition.
The distortion produced by TI precision op
amps is often below the measurement limit of commercially available distortion
analyzers. However, a special test circuit can be used to extend the measurement
capabilities.
Figure 3-1 shows a circuit that amplifies the op amp distortion to be
times (or approximately 40 dB) greater than that
normally produced by the op amp. Figure 3-2 shows the THD + N of the OPA1656 is below the theoretical noise floor of the
distortion analyzer. The purpose of the test circuit is to gain the THD + N of the
op amp above the distortion analyzer noise floor to measure the true performance of
the op amp. The addition of RA to the otherwise standard non-inverting
buffer amplifier configuration alters the feedback factor or noise gain of the
circuit. The closed-loop signal gain ACL is unchanged, but the feedback
available for error correction is reduced by a factor of
, thus extending the resolution by
or 40 dB. For further details see Section 6. Note that the input signal and load applied to the op amp are the same as with
conventional feedback without RA. When altering the noise gain, the gain
bandwidth product or GBW of the amplifier can be considered. A practical guideline
can be used when designing the test circuit noise gain. If the amplifier GBW is 10
MHz or greater a noise gain of
can be used. Amplifiers with a GBW less than 10 MHz
can use a noise gain of
. The value of RA is kept small to
minimize the effect on the distortion measurements and extraneous thermal noise.