SBOA590 November 2024 OPA186 , OPA206 , OPA328 , OPA391 , OPA928
Input bias current (IB) can be modeled as DC current sources on both the inverting and non-inverting input terminals (see Figure 2-1). This bias current develop an error voltage when it flows through the feedback network and source impedance. The error voltage can be referred to the input so that it adds to the VOS and VOS drift error sources. Equation 14 and Equation 15 shows the calculation for converting bias current into an offset voltage. Figure 2-2 and Equation 17 show how the input bias current translates into offset voltage sources.
The amplifier data sheet normally does not specify the bias current for the inverting and non-inverting input separately, but rather specifies the difference between the bias currents as bias current offset (IOS = IBP - IBN). If the bias currents are equal and the source impedance is equal to the feedback network impedance (RS = RF || RG), then the bias current offset voltages cancel (see Equation 19). However, in most modern precision amplifiers the bias currents have significant offset (IOS ≠ 0). In fact, for most CMOS amplifiers and many bipolar amplifiers the bias currents and bias offset are comparable in magnitude (IB ≈ IOS). Thus, the approach of balancing the source and feedback impedance frequently is not a practical way to minimize input offset voltage due to bias current. When IOS ≥ IB, the best approach to minimizing VIB is by minimizing RS, and RF || RG, not by balancing the source and feedback impedance. Equation 20 shows VIB where IOS is equal on both inputs (IBP = IB + IOS/2, and IBN = IB – IOS/2). The second term in this equation highlights how the IOS effects are not canceled when RS = RF || RG.
Equation 21 and Equation 22 are a good way to estimate the offset voltage due to bias current. These equations assume that half of the bias current offset is equally distributed between the inverting and non-inverting input. The two equations calculate the offset due to IB considering the polarity of the bias current offset (IOS is negative in Equation 21 and positive in Equation 22). For worst case error analysis calculate both values and select the largest absolute value (see Equation 23). Example 1 uses these equations in a calculation for maximum input offset voltage due to bias current for OPA205A.
Example 1: Calculation for OPA205 Maximum Bias Current to Input Offset Voltage
PARAMETER | TEST CONDITIONS | MIN | TYP | MAX | UNIT | ||
---|---|---|---|---|---|---|---|
IB | Input bias current | OPA205A | 25°C | ±0.1 | ±0.5 | nA | |
IOS | Input offset current | OPA205A | 25°C | ±0.1 | ±0.4 | nA |