SBOA597 November   2024 OPA928

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Architecture of Small Current Measurement
    1. 2.1 Coulombmeter
    2. 2.2 Using the Coulombmeter to Determine IB
    3. 2.3 Leakage of Integration Capacitor
  6. 3Benchmarking
    1. 3.1 Point to Point Wiring
    2. 3.2 Shielding
    3. 3.3 PCB Cleaning
    4. 3.4 Temperature Stability
  7. 4Calibration Using a Coulombmeter for Application Circuits
    1. 4.1 Calibration of Common Application Circuits
    2. 4.2 Calibration of Inverting Input
    3. 4.3 Calibration of Non-Inverting Input
    4. 4.4 Determine Resistance of the Capacitor Using Zero-Cross Method
    5. 4.5 Dielectric Absorption and Relaxation
    6. 4.6 Calibration at 85°C
    7. 4.7 Calibration at 25C
  8. 5Summary
  9. 6References

Dielectric Absorption and Relaxation

Capacitors are made of dielectric material with permittivity and dielectric loss. Permittivity and dielectric loss depend on frequency and temperature. In this case, frequency is super low, and temperature is stable.

A polypropylene capacitor was chosen for an integrator because of the high resistivity. Most polymer is a dielectric material. Dielectric material polarizes by the external electric field. There are several models of the polarizations that are electron cloud, ion of the atom and ion, and dipole orientation.

In this case, permittivity is increased as the movement of dipoles that follow the direction of the external electric field until aligning the orientation.

Dielectric relaxation is explained as a procedure of mechanical orientation. During the procedure of orientation, dipoles have resistance from the molecules around them, and orientation takes time to complete.

For a high-frequency electric field environment, the dipole cannot follow the change of the electric field as it is faster than the orientation process. Also, for low-frequency electric fields, dipole follows the change in the electric field without delay.

The electronic model of a capacitor with dielectric absorption is shown below. The model consists of multiple RC time constants in parallel. Due to parasitic capacitors and resistors with a very long time constant, the capacitor behaves as if the capacitor memorized the previous voltage.

 Parasitic Model of a
                    Capacitor Figure 4-15 Parasitic Model of a Capacitor

Dielectric absorption is standardized by IEC / EN 60384-1. According to the procedure of measurement, charge a capacitor at DC voltage for sixty minutes, followed by discharge for ten seconds. Then measure the voltage recovery for fifteen minutes, which indicates dielectric absorption voltage. The percentage of the voltage before and after is the level of the absorption. Polypropylene film capacitor has dielectric absorption of 0.05 to 0.1%.

Measuring ultra-low currents in the femtoampere range requires enough time for dielectric absorption and relaxation.

Figure 4-16 shows multiple cycles of integration measurements with a varying start voltage.

 Vcal Over Time With Zero-Cross
                    Method for Multiple Measurements Figure 4-16 Vcal Over Time With Zero-Cross Method for Multiple Measurements

Using the data in Figure 4-17 to calculate IB, we can see that the initial IB measurements vary significantly from the settled measurements. This effect is an additional error from the IB starts from different points and gradually aligns together as time goes by, which is Vcal goes up in this case. Though the relaxation process lasts long, we suppose the dielectric absorption was almost negligible at Vcal = 0.4V as the curves are aligned. With that, the slope of IB versus Vcal for Vcal is from 0.4V to 0.6V, indicating resistance. From the slope, the resistance is more likely as 16.2 x 1015Ω.

 IB Over Time With
                    Zero-Cross Method for Multiple Measurements Figure 4-17 IB Over Time With Zero-Cross Method for Multiple Measurements

At this point, we have only three parameters to consider. These are dielectric absorption, capacitor resistance, and IB as shown in the drawing.

 Model of the Three Parameters
                    in the Measured Area Figure 4-18 Model of the Three Parameters in the Measured Area

Estimate an error for the measured slope depending on what Vcal we took derivative. A calibration uses the resistance 16.2PΩ to provides 6aA leakage when the voltage across the capacitor is 100mV.

For example, if we measure the slope of the buffer (gain 10x) output is 10uV/sec, and Vcal is 1V which is the voltage across the integration capacitor of 100 [pF], IB is calculated as

10 x 10-6 / 10 x 100 x 10-12 = 100aA (without calibration)

10 x 10-6 / 10 x 100 x 10-12 + 0.1 / 16.2 x 10-15 = 106aA (with calibration).

 Configuration of Non-Inverting
                    Input Terminal Calibration With Leakage and Dielectric Absorption Figure 4-19 Configuration of Non-Inverting Input Terminal Calibration With Leakage and Dielectric Absorption

We can add or subtract leakage current to or from the measured number depending on the signs of Vcal and IB.