Since the introduction of the OPA593, the power operational amplifier (PA) has gained traction in the test and measurement sector. Specifically designed for Automated Test Equipment (ATE) applications, the OPA593 can drive output voltages up to 80V and output currents up to ±250mA, all within a compact 4mm × 4mm WSON package. The OPA593 operates across the full industrial temperature range of -40°C to 125°C, providing exceptional DC precision and robust output current limiting features that cater to diverse design requirements in ATE applications.
This application note demonstrates how to compensate for the OPA593 PA and current booster configuration, enabling output driving currents up to ±1A. Additionally, the document explains the implementation of the op amp’s dual feedback compensation techniques when driving capacitive loads of up to 1μF, making sure of adequate phase margin, stabilizing loop gains through AC analysis, and achieving fast step time responses in ATE applications.
All trademarks are the property of their respective owners.
The OPA593 is a high-voltage, high-output-current power amplifier (PA) that operates on an 85V single supply or a ±42.5V dual-supply configuration, with the capability to source or sink current up to ±250mA. This article focuses on dual-supply rail configurations, favored for their programmable and flexible precision voltage regulator setups commonly used in automated test equipment (ATE) applications. While the OPA593 meets the output voltage requirements for most power voltage regulator applications, OPA593 does not provide sufficient current drive in certain scenarios. In such cases, combining the OPA593 with a current booster topology can enhance the current drive capabilities while maintaining the amplifier’s overall operating voltage range, bandwidth, accuracy, and responsiveness to timing requirements.
In practice, a large capacitive load is often connected to the output of a power amplifier stage. Capacitive loads serve several purposes, including decoupling, filtering high-frequency noise, reducing voltage spikes, stabilizing transient responses, and improving output voltage regulation at the device under test (DUT). However, adding capacitive loads can introduce undesirable phase lag, potentially leading to loop instability in the power amplifier's feedback system.
Driving large capacitive loads presents significant design challenges for engineers, particularly in compensating for stability issues. This application note addresses these challenges when using the OPA593 with a Darlington current booster configuration. The document also explores the trade-offs associated with this technique, especially when driving capacitive loads up to 1µF.
Figure 1-1 and Table 2-2 present the schematic discussed in this application note, which aims to meet (or exceed) the design requirements.
Design Parameters | Composite Amplifier's Voltage Regulator Specifications |
---|---|
Input voltage range | Input swing up to ±5Vdc |
Output voltage range | Output swing up to ±40Vdc |
Output current range | OPA593 with current booster, driving up to ±1Adc |
Output impedance | RL ≥ 40Ω |
Closed-loop gains | 8V/V |
Open-loop output impedance | Open loop output impedance, Zo < approximately 1Ω |
Capacitive load | Low ESR (20mΩ), 1µF ceramic capacitive load and DUT |
Effective bandwidth | Approximately 50kHz, cutoff frequency at the –3dB point |
Step time behavior | Output rising/falling edge step-time response <100µs |
Output voltage accuracy | Approximately 0.05% or better across full scale |
The current booster’s open-loop output impedance and frequency response are among the key parameters in selecting a driver for ATE applications. The following criteria are summarized.
No | Current Booster Driver Selection Guide |
---|---|
1 | Low and consistent open-loop output impedance, with Zo variation over frequency in a given application. |
2 | Low distortion and high slew rate: Minimize crossover distortion while optimizing voltage biasing. |
3 | Meet source or sink current requirements for driving large capacitive and resistive loads. |
4 | Capability to withstand high power dissipation and effectively manage thermal stress under worst-case conditions. |
5 | Maximizing output voltage swing headroom relative to programmable power supply voltage rails. |
6 | Inclusion of output overvoltage and overcurrent protection features: overload, short-circuit, and current limiting. |
Line items 1 through 3 in Table 2-2 regarding the current booster are addressed in Sections 2 and 3 of the article.
In this design, the current booster is configured as a complementary push-pull Darlington topology with unity gain buffering. Figure 2-1 and Figure 2-2 demonstrate that the open-loop output impedance is regulated by a small bias voltage applied to the bases of the transistors. Forward biasing the base-emitter junction of the NPN transistor (T1) allows the booster to source positive voltage and current, while forward biasing the PNP transistor (T2) enables it to sink negative voltage and current. The bias voltage directly affects the open-loop output impedance; higher bias levels result in lower output impedance, as shown in Equation 1.
Where,
When the NPN transistor (T1) base-emitter junction is forward-biased, the current booster sources positive voltage and current at the output. Figure 2-1 illustrates the open-loop output impedance where the effects of ZCE ∥RL are shown to be less than 1Ω.
Conversely, when the emitter-base junction of the PNP transistor (T2) is forward-biased, the current booster sinks negative voltage and current at the output. Figure 2-2 demonstrates the open-loop output impedance, with the ZCE ∥RL effects yielding similar results. The combined open-loop output impedance remains consistent across the frequency range up to 1MHz.
The BJT transistor's forward biased voltage directly affects the open-loop output impedance; higher bias voltages lead to lower output impedance. The open-loop output impedance of the push-pull complementary BJT driver is primarily influenced by the output resistances (ro) of the NPN (rop) and PNP (ron) transistors, as well as the load resistance (RL). The open-loop output impedance of the Darlington current booster operates in parallel with RL, as illustrated in Equation 1.