SBOSA30D March 2022 – December 2024
PRODUCTION DATA
The accuracy of any current-sense amplifier is maximized by choosing the largest current-sense resistor value possible. A larger value sense resistor maximizes the differential input signal for a given amount of current flow and reduces the error contribution of the offset voltage. However, there are practical limits as to how large the current-sense resistor value can be in a given application because of the physical dimensions of the package, package construction, and maximum power dissipation. Equation 2 gives the maximum value for the current-sense resistor for a given power dissipation budget:
where:
An additional limitation on the size of the current-sense resistor and device gain is due to the power-supply voltage, VS, and device swing-to-rail limitations. To make sure that the current-sense signal is properly passed to the output, both positive and negative output swing limitations must be examined. Equation 3 provides the maximum values of RSENSE and GAIN to keep the device from exceeding the positive swing limitation.
where:
To avoid positive output swing limitations when selecting the value of RSENSE, there is always a trade-off between the value of the sense resistor and the gain of the device under consideration. If the sense resistor selected for the maximum power dissipation is too large, then selecting a lower gain device is possible to avoid positive swing limitations.
The negative swing limitation places a limit on how small the sense resistor value can be for a given application. Equation 4 provides the limit on the minimum value of the sense resistor.
where:
Table 8-1 shows an example of the different results obtained from using five different gain versions of the INA241x. From the table data, the highest gain device allows a smaller current-shunt resistor and decreased power dissipation in the element.
PARAMETER | EQUATION | RESULTS AT VS = 5V | |||||
---|---|---|---|---|---|---|---|
A1, B1 DEVICES | A2, B2 DEVICES | A3, B3 DEVICES | A4, B4 DEVICES | A5, B5 DEVICES | |||
G | Gain | 10V/V | 20V/V | 50V/V | 100V/V | 200V/V | |
VSENSE | Ideal differential input voltage | VSENSE = VOUT / G | 500mV | 250mV | 100mV | 50mV | 25mV |
RSENSE | Current sense resistor value | RSENSE = VSENSE / IMAX | 50mΩ | 25mΩ | 10mΩ | 5mΩ | 2.5mΩ |
PSENSE | Current-sense resistor power dissipation | RSENSE × IMAX2 | 5W | 2.5W | 1W | 0.5W | 0.25W |