SBOU124B march 2012 – july 2023 INA230
Users can connect voltage signals to the INA230 supply pin through Jumper J2. If J2 is set to the INT position, the VS pin is connected to the switchable VDUT signal generated from the SM-USB-DIG Platform. This voltage can be set to either 3.3 V or 5 V, depending on how it is configured in the software. While J4 is set in the INT position, the VS Power button in the INA230EVM software is able to control whether the VDUT supply voltage is turned on or off.
When J2 is set in the EXT position, an external supply connected to terminal T2 can be used to provide the supply voltage for the INA230.