SBOU128B february   2013  – july 2023 INA231

 

  1.   1
  2.   INA231EVM Evaluation Board and Software Tutorial
  3.   Trademarks
  4. 1Overview
    1. 1.1 INA231EVM Kit Contents
    2. 1.2 Related Documentation from Texas Instruments
  5. 2INA231EVM Hardware
    1. 2.1 Theory of Operation for INA231 Hardware
    2. 2.2 Signal Definitions of H1 (10-Pin Connector Socket)
      1. 2.2.1 Theory of Operation for SM-USB-DIG Platform
  6. 3INA231EVM (Rev A) Hardware Setup
    1. 3.1 Electrostatic Discharge Warning
    2. 3.2 Connecting the Hardware
    3. 3.3 Connecting Power
    4. 3.4 Connecting the USB Cable to the SM-USB-DIG Platform
    5. 3.5 INA231EVM Default Jumper Settings
    6. 3.6 INA231EVM Features
      1. 3.6.1 J2: I2C VS Control Setting
      2. 3.6.2 J3 and J4: I2C Address Hardware Setting (A0)
      3. 3.6.3 J5 and J6: I2C Address Hardware Setting (A1)
      4. 3.6.4 External I2C Lines and Terminal Block T1
      5. 3.6.5 VIN+ and VIN– Input filter (R1, R2, and C1)
      6. 3.6.6 Shunt Monitor Configuration and Terminal Blocks T3 and T4
  7. 4INA231EVM Software Setup
    1. 4.1 Operating Systems for the INA231EVM Software
    2. 4.2 Software Installation
  8. 5INA231EVM Software Overview
    1. 5.1 Starting the INA231EVM Software
    2. 5.2 Configuring the INA231EVM Software
      1. 5.2.1 I2C Address Selection
      2. 5.2.2 Configure Operating Mode
      3. 5.2.3 Set Conversion Times
      4. 5.2.4 Set Configuration Register
      5. 5.2.5 Configuring the Alert Pin
    3. 5.3 Using the INA231EVM Software
      1. 5.3.1 INA231 Bus Voltage, Shunt Voltage, Current, and Power Reading Bar
      2. 5.3.2 Calculation and Theory of Operation
      3. 5.3.3 Register Tab
      4. 5.3.4 Graph Tab
      5. 5.3.5 Auto-Write and the Supply Voltage
  9. 6INA231EVM Documentation
    1. 6.1 Schematic
    2. 6.2 PCB Layout
    3. 6.3 Bill of Materials
  10. 7Revision History

Software Installation

The INA231EVM software is included on the CD that is shipped with the EVM kit. The software is also available through the INA231EVM product folder on www.ti.com. To install the software to a computer, insert the disc into an available CD-ROM drive. Navigate to the drive contents and open theINA231EVM software folder. Locate the compressed file (INA231EVM.zip) and open it using WinZIP® or a similar file compression program; extract the INA231EVM files into a specific INA231EVM folder (for example, C:\INA231EVM) on your hard drive.

After the files are extracted, navigate to the INA231EVM folder created on the hard drive. Locate the setup.exe file and execute it to start the installation. The INA231 software installer file then begins the installation process as shown in Figure 4-1.

GUID-46BF8602-C49F-4573-8FCF-28622CC4218D-low.gifFigure 4-1 INA231EVM Software Installation

After the installation process initializes, the user is given the choice of selecting the directory in which to install the program; the default location is C:\Program Files\INA231\ and C:\Program Files\National Instruments\. Following this option, two license agreements are presented that must be accepted, as shown in Figure 4-2. After accepting the Texas Instruments and National Instruments license agreements, the progress bar opens and shows the installation of the software (see Figure 4-3). When the installation process is complete, click Finish.

GUID-3F14A2F6-CFCF-43C5-9130-391AA9EEC1E6-low.gifFigure 4-2 INA231EVM License Agreements
GUID-A5B0BD57-1648-45E6-A6BF-B7350B09F37E-low.gifFigure 4-3 INA231EVM Software Installation Progress