Use the serial COM port to read and write
registers through USB commands using the following format:
- Set device address format:
setdevice DEVID
- Where setdevice is always
lower case, and DEVID is defined as:
- SPI
- The chip
select number. Ex, for chip select of 3, use 3.
- I2C
- The 4 LSBs
of the address in decimal format. Ex, for an address of
0x4A, use 10.
- Note, when the SCB is reset
while one or more EVMs are connected, the address will default to the
lowest address/chip select found.
- The SCB checks for
I2C or SPI at start up, if no device is attached, it will
default to SPI. Reset the SCB with an I2C EVM connected to use
I2C.
- For example, to set an I2C
device with a register address of 0x4A you could send the command:
setdevice 10
- For this example, the EVM
would return the acknowledgment and state ("idle" or "collecting") in
JSON format:
- {"acknowledge":"setdevice 10"}
- {"evm_state":"idle"}
- Read register format: rreg ADR
- Where ADR is the address in
hex, and rreg is always lower case.
- Register addresses can be
in upper or lower case, and do not need to be led by '0x'. 0 padding
register addresses is also optional. For example, to read register
address 0xB, some valid commands include:
- rreg b
- rreg 0B
- rreg 0x0B
- When '0x'
is used, the 'x' must be lower case.
- For this example, the EVM
would return the results and state ("idle" or "collecting") in JSON format:
- {"acknowledge":"rreg 0x0B"}
- {"register":{"address":11,"value":3}}
- {"evm_state":"idle"}
- Write register format: wreg ADR VAL
- Where ADR and VAL are in
hex, and wreg is always lower case.
- Register addresses and
values can be in upper or lower case, and do not need to be led by '0x'.
0 padding register addresses and values is also optional. For example,
to write register address 0x1 with the value 0xfb69, some valid commands
include:
- wreg 1 fb69
- wreg 01 0xfb69
- wreg 0x01 0xFB69
- When '0x'
is used, the 'x' must be lower case.
- For this example, the EVM
would return the results and state ("idle" or "collecting") in JSON
format:
- {"acknowledge":"wreg 0x01 0xfb69"}
- {"console":"Writing 0xfb69 to ADC_CONFIG register"}
- {"evm_state":"idle"}