SBOU241E April 2020 – August 2022 INA228 , INA229 , INA237 , INA238 , INA239
To use the EVM with the SCB Controller (sold separately), connect the EVM as shown in Figure 4-1.
If using multiple EVMs, connect them as shown in Figure 4-2. Make sure to use a different chip select/address for each device. The GUI only supports one EVM/device type at a time, up to 4 EVMs total.