SBOU286A October 2022 – December 2022 INA350 , INA351
Figure 5-2 shows an example of how to set up the EVM for single-supply operation with a direct voltage connection to the reference (REF pin).
The following connections were made:
1. C9 and C10 are prepopulated with 0.1-µF power-supply decoupling capacitors. It is not required to remove C9 for proper single-supply operation. Refer to the device data sheet for additional power-supply decoupling information (Table 1-1).
2. A valid input common mode must be present on both inputs of the IA for proper operation.