SBOU297A April 2024 – July 2024
The AMP-PDK-EVM has hardware interfaces between the AMP-PDK-EVM, the daughtercard, and the device as seen earlier in Figure 2-1. The daughtercard can only be plugged in one way due to the metal alignment poles. The device can be plugged in several directions, therefore TI recommends to reference the figures below. Single channel daughtercards have a shutdown enable option via a header on the top right of the board. Refer to the corresponding device data sheet to determine which configuration to set the two-pin jumper to enable or disable shutdown mode.