SBOU309 august 2023 INA220
Firmware updates are pushed through the GUI if the previous driver was installed. If the GUI is downloaded for offline use, then the GUI can only update the SCB controller with the latest firmware available at the time of download. To check for the latest GUI or Firmware updates, launch the latest GUI version from the web browser.