SBOU311 October 2024 INA230
To use the EVM with the SCB Controller (sold separately), connect the EVM as shown in Figure 2-1.
If using multiple EVMs, then connect them as shown in Figure 2-2. Make sure to use a different I2C address for each device. The GUI only supports up to 4 EVMs total.