SBVU068 august 2023
The TPS7A78EVM-041 has completed pre-compliance testing for Conducted Emissions using two different input filters. Section 5.1.1 provides passing test results using resistors and capacitors only on the input of the TPS7A78. Section 5.1.2 provides passing test results using resistors, capacitors and inductors on the input of the TPS7A78.
The following is pre-compliance data that was grabbed from an oscilloscope. The Yellow curve is the Quasi-peak of the EVM; this curve needs to stay below the top red line, which is the limit for a passing test for the Quasi-peak voltage value. The green curve is the average voltage value of the EVM; this curve needs to stay below the bottom red line, which is the limit for a passing test for the average voltage value. Passing testing conditions are presented in the following sub-sections.