LeCroy is a trademark of Teledyne LeCroy.
Kapton is a registered trademark of DuPont.
All trademarks are the property of their respective owners.
The Texas Instruments TPS7A57EVM-056 evaluation module (EVM) helps designers evaluate the operation and performance of the TPS7A57 LDO voltage regulator. As shown in Table 1-1, the TPS7A57EVM-056 contains one TPS7A57 LDO voltage regulator in the RTE package. An optional load transient circuit is also included to assist the user with high-speed load transient testing.
EVM ORDERABLE NUMBER | VOUT | PART NAME | PACKAGE |
---|---|---|---|
TPS7A57EVM-056 | 0.5 V to 5.2 V | TPS7A5701RTE | 16-pin RTE |
This section describes the jumpers and connectors on the EVM, and how to properly connect, set up, and use the TPS7A57EVM-056. Section 2.1 and Section 2.3 describe the test setup and operation for the TPS7A57 LDO. Section 2.2 and Section 2.4 describe the test setup and operation of the optional load transient circuit.
VIN (J9) and GND (J10) are the connection terminals for the input supply. The VIN terminal is the positive connection, and the GND terminal is the negative (that is, ground) connection.
VOUT (J13) and GND (J14) are the connection terminals for the output load. The VOUT terminal is the positive connection, and the GND terminal is the negative (that is, ground) connection.