Prior to connecting the DC input
source, set the current limit of the input supply to 4A maximum. Make sure the
input source is initially set to 1.4V and connected to the VIN
connection point as shown in EVM Test Setup.
Additionally, if the load
transient is to be used, set the current limit of the VDD power
supply to 500mA maximum. Make sure the VDD source is initially set to
5.0V. Under no circumstances can the VDD voltage exceed
5.4V.
Connect voltmeter 1 at
VIN connection point to measure the input voltage.