SCEU027B November 2023 – October 2024 TPLD1201
PRODUCTION DATA
This user’s guide contains support documentation for the TPLD1201RWB evaluation module (EVM). Included is a description of how to set up and configure the EVM, how to use the EVM in conjunction with a TPLD-PROGRAM board, and how to use InterConnect Studio to configure the TPLD1201. Also included are the printed circuit board (PCB) layout, the schematic, and the bill of materials (BOM) of the TPLD1201-RWB-EVM.
TI only supports the use of the cables provided in the TPLD-PROGRAM kit to interface between the EVM and the programmer board.