SCEU028 November   2023

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Kit Contents
    2. 1.2 Features
  5. 2Hardware
    1. 2.1 PCB Overview
    2. 2.2 Hardware Setup
  6. 3Bill of Materials
  7. 4Revision History

Features

The TPLD-PROGRAM has the following features:

  • Interfaces with a computer running InterConnect Studio using a USB-to-Micro-USB Cable
  • Interfaces with TPLD EVMs using a 14-position cable
  • Compatible with all TPLD EVMs
  • Easy-to-use for programming and evaluation
  • Kit includes: Programmer board, USB cable, ribbon cable, board case, and a quick start guide

Quick Troubleshooting

The following table shows some common issues while configuring TPLD with the TPLD-PROGRAM, as well as how to diagnose and fix these issues. If you are having an issue using the TPLD-PROGRAM to configure a TPLD and are not able to fix the issue using this list, TI recommends posting on E2E.TI.com for help from our engineering team.

Indication Issue Solution
No blue LEDs light up when TPLD-PROGRAM is plugged into a computer Poor connection between the TPLD-PROGRAM and the computer Unplug USB connection between the TPLD and the computer. Check both plugs for obstructions before plugging in the cable again.
InterConnect Studio does not recognize the TPLD-PROGRAM attached to the computer Poor connection between the TPLD-PROGRAM and the computer Unplug the 14-position ribbon cable between the TPLD and the computer. Check both headers for obstructions before plugging in the cable again.
InterConnect Studio does not recognize the TPLD connected to the output of the TPLD-PROGRAM Poor connection between the TPLD-PROGRAM and the TPLD EVM Unplug the 14-position ribbon cable between the TPLD and the computer. Check both headers for obstructions before plugging in the cable again.