SCEU031B August   2024  – October 2024 TPLD801

PRODUCTION DATA  

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Functional Blocks
      1. 2.1.1 Test Points
      2. 2.1.2 Programmer Header Block (P1)
      3. 2.1.3 External Connection Header Block
      4. 2.1.4 GPI Protection Block
      5. 2.1.5 DRL Socket
      6. 2.1.6 SW or LED Testing Blocks
      7. 2.1.7 GPI Switch Testing Block
  9. 3Software
    1. 3.1 Using the TPLD801-DRL-EVM
      1. 3.1.1 Equipment Needed for Programming
      2. 3.1.2 Installing Software
    2. 3.2 Configuring a TPLD Device
      1. 3.2.1 TPLD801-DRL-EVM Setup for Programming
      2. 3.2.2 Inserting a TPLD801DRL into the DRL Socket
      3. 3.2.3 Connecting the TPLD801-DRL-EVM to a TPLD-PROGRAM Board
      4. 3.2.4 Temporarily Configuring a TPLD Device
      5. 3.2.5 Permanently Programming a TPLD Device
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layout
      1. 4.2.1 PCB Overview
    3. 4.3 Bill of Materials
  11. 5Additional Information
    1. 5.1 Trademarks
  12. 6Revision History

Temporarily Configuring a TPLD Device

This section covers using InterConnect Studio to configure a TPLD801.

When the TPLD is temporarily configured, removing power from the device causes the TPLD to reset and the configured circuit to be erased. The TPLD can be reconfigured multiple times without needing to be reset between configurations.

  1. Open InterConnect Studio on the computer to which the TPLD-PROGRAM is connected. Under Design, select TPLD801. Under Package:, select DRL (SOT-5X3, 8).
  2. Select Empty Design to build a custom circuit, or select one of the premade demo circuits.
    TPLD801-DRL-EVM Selecting TPLD801DRL
                            in ICS Figure 3-5 Selecting TPLD801DRL in ICS
  3. InterConnect Studio opens the chosen circuit.
  4. Select the thee dots icon next to Configure TPLD801 and make sure that the Permanently Configure Device is unchecked.
  5. Select CONFIGURE TPLD801 in the top left corner of InterConnect Studio to configure the TPLD in the socket of the EVM with the circuit shown by InterConnect Studio. Select the serial port connected to the TPLD-PROGRAM, then select OK.
    TPLD801-DRL-EVM Temporarily Configuring in ICSFigure 3-6 Temporarily Configuring in ICS
    1. Some LEDs on the TPLD801-DRL-EVM can flash during the programming sequence, which is normal.
    2. If the configuration fails, check the connections between the EVM and the computer, make sure SW8 is ON, check the connection between the TPLD device and the socket contacts, confirm that the shunt setup is correct according to Section 3.2.1 and retry.

Once the programming sequence is completed, the TPLD device on the board is temporarily configured with the circuit built in InterConnect Studio. The configured circuit can be tested using the buttons and LEDs provided on the EVM.