SCEU031B August 2024 – October 2024 TPLD801
PRODUCTION DATA
The TPLD801 is part of the TI Programmable Logic Device (TPLD) family of devices that feature versatile programmable logic ICs with combinational logic and sequential logic functions. TPLD provides an integrated, compact, low power design to implement common system functions, such as timing delays, system resets, power sequencers, I/O expanders, and more.
This user’s guide contains support documentation for the TPLD801DRL evaluation module (EVM). Included is a description of how to set up and configure the EVM, how to use the EVM in conjunction with a TPLD-PROGRAM board, and how to use InterConnect Studio to configure TPLD801. Also included are the printed circuit board (PCB) layout, the schematic, and the bill of materials (BOM) of the TPLD801-DRL-EVM.
TI only supports the use of the cables provided in the TPLD-PROGRAM kit to interface between the EVM and the programmer board.