SFFS053 December 2021 TPS272C45
This section provides a Failure Mode Analysis (FMA) for the pins of the TPS272C45. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the TPS272C45 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS272C45 data sheet.
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT1 |
1, 2, 3 |
Current limit of the device engages and thermal protection turns off the Channel 1 (OUT1) FET |
B |
NC |
4, 22 |
No effect |
D |
OUT2 |
5, 6, 7 |
Current limit of the device engages and thermal protection turns off the Channel 1 (OUT1) FET |
B |
VS |
8, 9, 23, 24 |
The output stages are not powered and the FET does not turn ON |
B |
FLT (version A, B, C) |
10 |
Fault status reported can be erroneous |
B |
FLT1 (version D) |
10 |
Fault status reported can be erroneous |
B |
SNS |
11 |
SNS current or fault status reported on the SNS pin is erroneous |
B |
DIA_EN |
12 |
Diagnostics including current sense and fault reporting does not function |
B |
SEL |
13 |
If DIA_EN high then channel 1's sense current output always on SNS |
B |
LATCH |
14 |
Device defaults to auto-retry mode when encountering thermal fault |
B |
EN1 |
15 |
Channel 1 FET is turned off |
B |
EN2 |
16 |
Channel 2 FET is turned off |
B |
GND |
17 |
Any GND network connected for protection is bypassed |
B |
ILIMD (version A, B, C) |
18 |
The threshold for current limit is set by ILIMx pin for the entire duration after the channel is enabled. The higher or lower current limit setting for a period after enable and the delay duration does not function |
B |
FLT2 (version D) |
18 |
Fault status reported can be erroneous |
B |
VDD (Version A, C, D) |
19 |
Version A, C, D: If an external supply is connected (that is, not grounded) , the device switches to powering all blocks from VS supply – loss of output state for a period and an increase in current draw from VS supply |
B |
GND (Version B) |
19 |
Version B: no effect |
D |
ILIMx |
20, 21 |
The current limit protection switches to a level set internally at a higher level |
B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT1 |
1, 2, 3 |
If any one pin is open, an increase in switch resistance. If all pins are open, OUT1 is high impedance |
B |
NC |
4, 22 |
No effect |
D |
OUT2 | 5, 6, 7 | If any one pin is open, an increase in switch resistance. If all pins are open, OUT1 is high impedance |
B |
VS | 8, 9, 23, 24 | If any one pin is open, an increase in switch resistance. If all pins are open, output stage power supply input is lost and output switches do not function. |
B |
FLT (version A, B, C) |
10 |
Fault condition cannot be reported |
B |
FLT1 (version D) |
10 | Fault condition on channel 1 cannot be reported |
B |
SNS |
11 |
No current out of the SNS pin, no current sense functionality |
B |
DIA_EN |
12 |
Pin pulled low internally, diagnostics including current sense and fault reporting does not function |
B |
SEL |
13 | Pin pulled low internally, diagnostics including current sense and fault reporting is for Channel 1 only |
B |
LATCH |
14 | Pin pulled low internally, device defaults to auto-retry mode when encountering thermal fault |
B |
EN1 |
15 | Pin pulled low internally, Channel 1 FET is turned off |
B |
EN2 |
16 | Pin pulled low internally, Channel 2 FET is turned off |
B |
GND |
17 |
The output FETs are off and the device supply and functionality is lost |
B |
ILIMD (version A, B, C) |
18 |
The current limit configuration and delay during the initial phase after enable defaults to > 40 kohm |
B |
FLT2 (version D) |
18 | Fault condition on Channel 2 cannot be reported |
B |
VDD (Version A, C, D) |
19 | Version A, C, D: If an external supply is connected (i.e. Not grounded) , the device switches to powering all blocks from VS supply - loss of output state for a period and an increase in current draw from VS supply |
B |
GND (Version D) |
19 | Version B: no effect |
D |
ILIMx |
20, 21 | The current limit protection switches to a level set internally at a higher level |
B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
OUT1 | 1, 2, 3 |
NC |
No effect |
D |
NC |
4 |
OUT2 |
No effect |
D |
OUT2 |
5, 6, 7 |
N/A |
Not plausible (corner pin) |
D |
VS |
8, 9 |
FLT (versions A, B, C) |
Fault condition cannot be reported |
B |
VS |
8, 9 |
FLT1 (version D) |
Fault condition on Channel 1 cannot be reported |
B |
FLT1 or FLT |
10 |
SNS |
SNS current output is affected, fault condition not reported correctly |
B |
SNS |
11 |
DIA_EN |
SNS current output affected, diagnostic functionality affected. |
B |
DIA_EN |
12 |
N/A | Not plausible (corner pin) |
B |
SEL |
13 |
LATCH |
Diagnostic functionality affected, as well as auto-retry and latch on thermal fault behavior |
B |
LATCH |
14 |
EN1 |
The output state on Channel 1 can be affected |
B |
EN1 |
15 |
EN2 | The output state on Channel 1 or Channel 2 can be affected |
B |
EN2 |
16 |
GND | The output on Channel 2 cannot be turned ON |
B |
GND |
17 |
ILIMD (Versions A, B, C) |
The threshold for current limit is set by ILIMx pin for the entire duration after the channel is enabled. The higher or lower current limit setting for a period after enable and the delay duration does not function |
B |
GND |
17 |
FLT2 (Version D) | Fault status reported on Channel 2 can be erroneous |
B |
ILIMD (Versions A, C) |
18 |
VDD (Version A, C) |
The current limit behavior on enable is affected, additional current draw from VDD supply, if connected. |
B |
ILIMD (Version B) |
18 |
GND (Version B) | The threshold for current limit is set by ILIMx pin for the entire duration after the channel is enabled. The higher or lower current limit setting for a period after enable and the delay duration does not function |
B |
FLT2 (Version D) |
18 |
VDD (Version D) |
Fault status reported on Channel 2 can be erroneous |
B |
VDD (Version A, C, D) |
19 |
N/A | Not plausible (corner pin) |
B |
VDD (Version B) |
19 |
N/A | Not plausible (corner pin) |
B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT1 |
1, 2, 3 |
The channel 1 output cannot be turned off, OUT1 connected to VS |
B |
NC |
4, 22 |
No effect |
D |
OUT2 |
5, 6, 7 |
The channel 2 output cannot be turned off, OUT2 connected to VS |
B |
VS |
8, 9, 23, 24 |
No effect |
D |
FLT (versions A, B, C) |
10 |
Fault status reported can be erroneous |
B |
FLT1 (version D) |
10 |
Fault status reported can be erroneous |
B |
SNS |
11 |
SNS pin current or fault status reported can be erroneous |
B |
DIA_EN |
12 |
Diagnostics are constantly enabled |
B |
SEL |
13 |
If DIA_EN high then channel 2's sense current output always on SNS |
B |
LATCH |
14 |
Device defaults to latch mode when encountering thermal fault |
B |
EN1 |
15 |
Channel 1 FET is turned ON, output cannot be turned OFF |
B |
EN2 |
16 |
Channel 2 FET is turned ON, output cannot be turned OFF |
B |
GND |
17 |
The output stages are not powered and the FET does not turn ON |
B |
ILIMD (Version A, B, C) |
18 |
The current limit behavior on enable is erroneous, potential violation of absolute maximum rating of pin and possible breakdown of ESD cell |
A |
FLT2 (Version D) |
18 |
Fault status reported can be erroneous, potential violation of absolute maximum rating of pin and possible breakdown of ESD cell |
A |
VDD (Version A, C, D) |
19 |
Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell and loss of full device functionality |
A |
GND (Version B) |
19 |
Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell and loss of full device functionality |
A |
ILIMx |
20, 21 |
Potential violation of absolute maximum rating of pin and possible breakdown of ESD cell and loss of all functionality |
A |