SFFS137 April 2021 LDC3114-Q1
This section provides a Failure Mode Analysis (FMA) for the pins of the LDC3114-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the LDC3114-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the LDC3114-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Device is powered within published absolute maximum operating conditions.
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
COM |
1 |
COM is grounded without a bypass capacitor. Will cause an error in sensor input and unpredictable LC sensor behavior |
B |
GND |
2 |
Normal operation |
D |
LPWRB |
3 |
Device stuck in Low Power Mode |
B |
VDD |
4 |
Power supply shorted to ground |
B |
INTB |
5 |
INTB is stuck low |
B |
IN3 |
6 |
No LC sensor input |
B |
IN2 |
7 |
No LC sensor input |
B |
IN1 |
8 |
No LC sensor input |
B |
IN0 |
9 |
No LC sensor input |
B |
GND |
10 |
Normal operation |
D |
OUT3 |
11 |
May result in output status error |
B |
OUT2 |
12 |
May result in output status error |
B |
OUT1 |
13 |
May result in output status error |
B |
SDA |
14 |
SDA will be stuck low. I2C read/write will be non-functional |
B |
OUT0 |
15 |
May result in output status error |
B |
SCL |
16 |
SCL will be stuck low. I2C read/write will be non-functional |
B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
COM |
1 |
No common return path for LC resonator sensors |
B |
GND |
2 |
No power supply to device |
B |
LPWRB |
3 |
Failure to set functional mode |
B |
VDD |
4 |
No power supply to device |
B |
INTB |
5 |
INTB does not assert for button presses or error conditions |
B |
IN3 |
6 |
No LC sensor input |
B |
IN2 |
7 |
No LC sensor input |
B |
IN1 |
8 |
No LC sensor input |
B |
IN0 |
9 |
No LC sensor input |
B |
GND |
10 |
No power supply to device |
B |
OUT3 |
11 |
Output is not connected to a load. May result in output status error |
B |
OUT2 |
12 |
Output is not connected to a load. May result in output status error |
B |
OUT1 |
13 |
Output is not connected to a load. May result in output status error |
B |
SDA |
14 |
I2C read/write will be non-functional |
B |
OUT0 |
15 |
Output is not connected to a load. May result in output status error. |
B |
SCL |
16 |
I2C read/write will be non-functional |
B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
COM |
1 |
GND |
COM is grounded without a bypass capacitor. Will cause an error in sensor input and unpredictable LC sensor behavior |
B |
GND |
2 |
LPWRB |
Device stuck in Low Power Mode |
B |
LPWRB |
3 |
VDD |
Device stuck in Normal Power Mode |
B |
VDD |
4 |
INTB |
INTB stuck high; loss of INTB functionality |
B |
INTB |
5 |
IN3 |
Loss of INTB
functionality and error in sensor input |
B |
IN3 |
6 |
IN2 |
Error in LC sensor input |
B |
IN2 |
7 |
IN1 |
Error in LC sensor input |
B |
IN1 |
8 |
IN0 |
Error in LC sensor input |
B |
IN0 |
9 |
GND |
No LC sensor input |
B |
GND |
10 |
OUT3 |
May result in output status error |
B |
OUT3 |
11 |
OUT2 |
May result in output status error |
B |
OUT2 |
12 |
OUT1 |
May result in output status error |
B |
OUT1 |
13 |
SDA |
May result in output status error |
B |
SDA |
14 |
OUT0 |
I2C read/write will be non-functional |
B |
OUT0 |
15 |
SCL |
May result in output status error and I2C read/write will be non-functional |
B |
SCL |
16 |
COM |
I2C read/write will be non-functional |
B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
COM |
1 |
Will cause unpredictable LC sensor behavior |
B |
GND |
2 |
Power supply shorted to ground |
B |
LPWRB |
3 |
Device stuck in Normal Power Mode |
B |
VDD |
4 |
Normal operation |
D |
INTB |
5 |
Loss of INTB functionality |
B |
IN3 |
6 |
No LC sensor input |
B |
IN2 |
7 |
No LC sensor input |
B |
IN1 |
8 |
No LC sensor input |
B |
IN0 |
9 |
No LC sensor input |
B |
GND |
10 |
Power supply shorted to ground |
B |
OUT3 |
11 |
Error in logic output |
B |
OUT2 |
12 |
Error in logic output |
B |
OUT1 |
13 |
Error in logic output |
B |
SDA |
14 |
I2C read/write will be non-functional |
B |
OUT0 |
15 |
Error in logic output |
B |
SCL |
16 |
I2C read/write will be non-functional |
B |