All trademarks are the property of their respective owners.
This document contains information for OPA858-Q1 (WSON-8 package) to aid in a functional safety system design. Information provided are:
OPA858-Q1 shows the device functional block diagram for reference.
OPA858-Q1 was developed using a quality-managed development process, but was not developed in accordance with the IEC 61508 or ISO 26262 standards.
This section provides Functional Safety Failure In Time (FIT) rates for OPA858-Q1 based on two different industry-wide used reliability standards:
FIT IEC TR 62380 / ISO 26262 | FIT (Failures Per 109 Hours) |
---|---|
Total Component FIT Rate | 5 |
Die FIT Rate | 3 |
Package FIT Rate | 2 |
The failure rate and mission profile information in Table 2-1 comes from the Reliability data handbook IEC TR 62380 / ISO 26262 part 11:
Table | Category | Reference FIT Rate | Reference Virtual TJ |
---|---|---|---|
4 | BICMOS Op Amp, Comparators, Voltage Monitors | 4 | 45°C |
The Reference FIT Rate and Reference Virtual TJ (junction temperature) in Table 2-2 come from the Siemens Norm SN 29500-2 tables 1 through 5. Failure rates under operating conditions are calculated from the reference failure rate and virtual junction temperature using conversion information in SN 29500-2 section 4.
This section provides a Failure Mode Analysis (FMA) for the pins of the OPA858-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 3-2 through Table 3-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 3-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 3-1 shows the OPA858-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the OPA858-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
1 | FB | May cause device to overheat. | A |
2 | NC | No internal connection to die; normal operation. Not recommended because of potential coupling. | C |
3 | IN- | Input at VS- (GND) is valid input; however, desired application result is unlikely. | C |
4 | IN+ | Input at VS- (GND) is valid input; however, desired application result is unlikely. | C |
5 | VS- | Normal operation, unless dual supply voltage was intended. | D |
6 | OUT | May cause device to overheat. | A |
7 | VS+ | Diodes from input to VS+ may turn on due to input signal and cause electrical overstress (EOS). | A |
8 | PD | Power-down connection is set to logic low. Amplifier is disabled, output is placed in a high-impedance state, and power consumption is reduced. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
1 | FB | Feedback pin can be left open. There is no effect on the IC, since the pin is internally connected to the output of the amplifier. | C |
2 | NC | No internal connection to die; normal operation. Leaving this pin floating leads to best overall application performance. | D |
3 | IN- | Floating input; circuit will likely not function as expected. | C |
4 | IN+ | Floating input; circuit will likely not function as expected. | C |
5 | VS- | Lowest voltage pin will try to power the device's VS- pin. | B |
6 | OUT | Output can be left open. There is no effect on the IC, but the output will not be measured. | C |
7 | VS+ | Highest voltage pin will try to power the device's VS+ pin. | B |
8 | PD | Power-down pin can be left open. The pin will be pulled to VS+ through the internal 75 kΩ, which will enable the amplifier. This is not recommended because of potential coupling. | C |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
1 | FB | NC | NC has no internal connection to die, and FB is internally connected to the output of the amplifier. There is no damage to device, but circuit might not function as expected. | C |
2 | NC | IN- | No damage to device. Application circuit will not work. | C |
3 | IN- | IN+ | No damage to device. Application circuit will not work. | C |
4 | IN+ | VS- | Input at VS- (GND) is valid input; however, desired application result is unlikely. Pins are not adjacent to each other. | C |
5 | VS- | OUT | May cause device to overheat. | A |
6 | OUT | VS+ | May cause device to overheat. | A |
7 | VS+ | PD | Power-down connection is set to logic high. Amplifier is enabled and operates normally. | D |
8 | PD | FB | Depending on the voltage at the output of the amplifier, the amplifier might be disabled or enabled following the voltage threshold specified in the device data sheet. Pins are not adjacent to each other. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
1 | FB | May cause device to overheat. | A |
2 | NC | No internal connection to die; normal operation. Not recommended because of potential coupling. | C |
3 | IN- | Input at VS+ is a valid input; however, desired application result is unlikely. | C |
4 | IN+ | Input at VS+ is a valid input; however, desired application result is unlikely. | C |
5 | VS- | Diodes from input to VS- may turn on due to input signal and cause electrical overstress (EOS). | A |
6 | OUT | May cause device to overheat. | A |
7 | VS+ | Normal operation. | D |
8 | PD | Power-down connection is set to logic high. Amplifier is enabled and operates normally. | D |