All trademarks are the property of their respective owners.
This document contains information for the OPAx607-Q1 (DBV and DGK packages) to aid in a functional safety system design. The DBV package corresponds to the single-channel amplifier, while the DGK package corresponds to the dual-channel amplifier. Information provided are:
Figure 1-1 shows the device functional block diagram for reference.
The OPAx607-Q1 was developed using a quality-managed development process, but was not developed in accordance with the IEC 61508 or ISO 26262 standards.