SFFS700 May 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
LIN module supports detection of Physical Bus Error condition, an error flag is set and interrupt generated. A Physical Bus Error (PBE) is detected by a master if no valid message can be generated on the bus (Bus shorted to GND or VBAT). The bit monitor detects a PBE during the header transmission if a Synch Break cannot be generated (for example, because of a bus shortage to VBAT) or if a Synch break Delimiter cannot be generated (for example, because of a bus shortage to GND).